Part Number: MSP430G2230-EP
Other Parts Discussed in Thread: MSP430G2230
I'm essentially using this microcontroller as a co-processor for a different micro, and want to make sure my choice of selection here is the correct one.
These are the needs I have:
1. Wakeup MSP on UART RX activity <- needs to not miss ANY bytes that came in to trigger the wakeup at 9600baud
2. Trigger an interrupt pin on RX activity
3. Re-host "buffered" received UART data to main processor via I2C.
4. Go back to sleep after I2C data is sent
5. 3.3V supply power
Given my needs above, do I have the correct choice of MSP selected? Any and all feedback would be greatly appreciated, thank you!