Part Number: MSP430F5438A
Other Parts Discussed in Thread: MAX232, MSP430F5529
Hello, Texas Team or Experts
My MCU have to communicate RS232 with MSP430F5438A.
So, I found the example of uart loopback in CCS Resource Explorer and then I downloaded firmware.
But, there are problems. Terminal didn't work using Hercules or CCS.
Also if I set transmitData = 'a', I hook up TX(TX-GND) or RX(RX-GND) with an oscilloscope, but the data value didn't check.
where is the problem?
I designed MCU and RS232(with usb)

Board : MSP-TS430PZ5x100 (MSP430F5438A)
Code :
//******************************************************************************
//! This example shows how to configure the UART module as the loopback to
//! verify that received data is sent data.
//!
//! MSP430F5438A
//! -----------------
//! RST -| P3.4/UCA0TXD|----|
//! | | |
//! | | |
//! | P3.5/UCA0RXD|----|
//! | |
//!
//!
//! This example uses the following peripherals and I/O signals. You must
//! review these and change as needed for your own board:
//! - UART peripheral
//! - GPIO Port peripheral (for UART pins)
//! - UCA0TXD
//! - UCA0RXD
//!
//! This example uses the following interrupt handlers. To use this example
//! in your own application you must add these interrupt handlers to your
//! vector table.
//! - USCI_A0_VECTOR.
//******************************************************************************
#include "driverlib.h"
//*****************************************************************************
//
//Select Baud rate
//
//*****************************************************************************
#define BAUD_RATE 9600
//*****************************************************************************
//
//Initialize received data
//
//*****************************************************************************
uint8_t receivedData = 0x00;
//*****************************************************************************
//
//Initialize transmit data
//
//*****************************************************************************
uint8_t transmitData = 0x00;
uint8_t check = 0;
void main (void)
{
//Stop WDT
WDT_A_hold(WDT_A_BASE);
//P3.4,5 = USCI_A0 TXD/RXD
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P3, GPIO_PIN4 + GPIO_PIN5);
//Baudrate = 9600, clock freq = 1.048MHz
//UCBRx = 109, UCBRFx = 0, UCBRSx = 2, UCOS16 = 0
USCI_A_UART_initParam param = {0};
param.selectClockSource = USCI_A_UART_CLOCKSOURCE_SMCLK;
param.clockPrescalar = 109;
param.firstModReg = 0;
param.secondModReg = 2;
param.parity = USCI_A_UART_NO_PARITY;
param.msborLsbFirst = USCI_A_UART_LSB_FIRST;
param.numberofStopBits = USCI_A_UART_ONE_STOP_BIT;
param.uartMode = USCI_A_UART_MODE;
param.overSampling = USCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION;
if (STATUS_FAIL == USCI_A_UART_init(USCI_A0_BASE, ¶m)){
return;
}
//Enable UART module for operation
USCI_A_UART_enable(USCI_A0_BASE);
//Enable Receive Interrupt
USCI_A_UART_clearInterrupt(USCI_A0_BASE, USCI_A_UART_RECEIVE_INTERRUPT);
USCI_A_UART_enableInterrupt(USCI_A0_BASE, USCI_A_UART_RECEIVE_INTERRUPT);
__bis_SR_register(GIE);
while (1)
{
transmitData = transmitData+1; // Increment TX data
// Load data onto buffer
USCI_A_UART_transmitData(USCI_A0_BASE,
transmitData);
while(check != 1);
check = 0;
}
}
//******************************************************************************
//
//This is the USCI_A0 interrupt vector service routine.
//
//******************************************************************************
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR (void)
{
switch (__even_in_range(UCA0IV,4)){
//Vector 2 - RXIFG
case 2:
receivedData = USCI_A_UART_receiveData(USCI_A0_BASE);
if(!(receivedData == transmitData)) // Check value
{
while(1);
}
check =1;
break;
default: break;
}
}
or address : https://dev.ti.com/tirex/explore/node?node=AHTWzeTf6uwMxTvmqYEvag__IOGqZri__LATEST // 
Can Someone help me?