Hi experts,
Is it possible to connect a 38.4kHz crystal to XT1 with MSP430FR2153 (FR2xx series Clock System)?
My customer wants to do UART communication, but the device to connect to is fixed at 4800 bps. We believe that if we input a 38.4kHz crystal to ACLK=BCLK, we can theoretically communicate with an error rate of TX=±0%, RX=±6.25%. (This is when the accuracy of the crystal is ignored.)
I understand from the user's guide "NOTE: XT1 in HF mode configuration" that the input cannot exceed 40 kHz.
Best regards,
O.H