Other Parts Discussed in Thread: MSP430F5438A
I am having issues with sending bytes of data back and forth between a computer and
an MSP430. This is the code segments that I am using to handle the serial port on an MSP430F5438A
experimenter board.First is the write serial function:
void write_serial(char data){
while(!(UCA1IFG&UCTXIFG)){} //wait for empty transmit buffer
UCA1TXBUF=data; //load data
}
next is an interrupt to read the serial port (buffer stores bytes, buffer_ptr is incremented):
//serial port interrupt handler
#pragma vector=USCI_A1_VECTOR
__interrupt void USCI_A1_ISR (void)
{
/*commands:
* turn pump (p) on/off (s) is 00000001 ppppssss, returns 00110011
* turn three_way (t) on/off (s) is 00000010 ttttssss, returns 00110011
* read sensor (s) 00000011 ssssssss, returns 00110011
* set selector (p) 00000100 pppppppp, returns 00110011
* home selector() 00000101 00000000, returns 00110011
* reset() 00000110 00000000, returns 00110011
* off() 00000111 00000000, returns 00110011
* bias_sensor_gate(g,double) 00001000 double, returns 00110011
* bias_sensor_drain(d,double) 00001001 double, returns 00110011
* set_pressure(double pres) 00001010 double , returns 00110011
* turn two_way (t) on/off (s) is 00001011 ttttssss, returns 00110011
* */
//buffer[buffer_ptr] holds latest data
buffer[buffer_ptr]=UCA1RXBUF;
buffer_ptr++;
__bic_SR_register_on_exit(LPM3_bits);
}
next is the initialization:
//init serial port
P10DIR|=0x01; //reset USB
P10OUT&=!0x01;
for(i=0;i<100;i++){}
P10OUT|=0x01;
UCA1CTL1|=UCSWRST; //reset
P5SEL|=BIT7|BIT6;
P5DIR|=BIT6; //transmit
P5DIR&=!BIT7; //receive
//general settings
UCA1CTL0 = UCMODE_0; //all zeros
UCA1CTL0 &= ~UC7BIT; // 8bit char
UCA1CTL1 |= UCSSEL_1; //ACLK
//set up baud rate
UCA1BR0=3; //reasonably close to 9600 baud
UCA1BR1=0;
UCA1MCTL=6;
UCA1CTL1 &= ~UCSWRST;
UCA1IE|=UCRXIE;
Next is the test function that I am using, probably where the problem is:
void test_receive_str(){
int i;
//write_serial(READY);
//expect to receive 10 bytes from scilab test program
//then dump them out
clear_buffer();
do{
write_serial(READY);
}while(buffer[0]!=ACK);
if(buffer_ptr>=10){
for(i=0;i<10;i++)
write_serial(buffer[i]);
clear_buffer();
}
write_serial(DONE);
//disable serial port, go to uca3
P10SEL|=0x01;
P10OUT&=!0x01;
}
Any advice?...