Part Number: MSP430F5438A
Hi, everyone.
I'm new to the I2C protocol, and have no experience programming for it.
I have read I2C communication in MSP430 Microcontroller basics book by David.john. Also i have looked CCS example code.
However i havn't been able to make a connection with my MCU.
My Board is MSP-TS430PZ5x100 using MSP430F5438A.
I want to communicate I2C using my board. So i have set USCI_B0 as master and transmission, and I set USCI_B1 as slave and wrote a code to receive it.
but My code started repeating itself in 21 lines.
void USCI_B_I2C_masterSendSingleByte (uint16_t baseAddress,
uint8_t txData
)
{
//Store current TXIE status
uint8_t txieStatus = HWREG8(baseAddress + OFS_UCBxIE) & UCTXIE;
//Disable transmit interrupt enable
HWREG8(baseAddress + OFS_UCBxIE) &= ~(UCTXIE);
//Send start condition.
HWREG8(baseAddress + OFS_UCBxCTL1) |= UCTR + UCTXSTT;
//Poll for transmit interrupt flag.
while (!(HWREG8(baseAddress + OFS_UCBxIFG) & UCTXIFG)) ;
//Send single byte data.
HWREG8(baseAddress + OFS_UCBxTXBUF) = txData;
//Poll for transmit interrupt flag.
while (!(HWREG8(baseAddress + OFS_UCBxIFG) & UCTXIFG)) ;
//Send stop condition.
HWREG8(baseAddress + OFS_UCBxCTL1) |= UCTXSTP;
//Clear transmit interrupt flag before enabling interrupt again
HWREG8(baseAddress + OFS_UCBxIFG) &= ~(UCTXIFG);
//Reinstate transmit interrupt enable
HWREG8(baseAddress + OFS_UCBxIE) |= txieStatus;
}
This is my Code using driverlib.h.
#include <MSP430.h>
#include <MSP430F5xx_6xx/driverlib.h>
uint8_t transmitData = 0x52;
uint8_t receiveData;
/**
* main.c
*/
void main(void)
{
WDT_A_hold(WDT_A_BASE);// stop watchdog timer
initGPIO();
initClock();
initI2C();
while(1)
{
USCI_B_I2C_masterSendSingleByte(USCI_B0_BASE, transmitData);
while(USCI_B_I2C_isBusBusy(USCI_B0_BASE));
__delay_cycles(50);
transmitData++;
}
}
#pragma vector = USCI_B1_VECTOR
__interrupt void USCI_B1_ISR(void)
{
switch(__even_in_range(UCB1IV, 0x0C)){
case 0x0C:
receiveData = USCI_B_I2C_slaveGetData(USCI_B1_BASE);
break;
default: //__never_executed();
break;
}
}
#include <MSP430F5xx_6xx/driverlib.h>
uint32_t myACLK, mySMCLK, myMCLK;
void initGPIO(void)
{
//Configurate oscillator
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P7, GPIO_PIN0 + GPIO_PIN1);
//Configurate I2C
GPIO_setAsPeripheralModuleFunctionInputPin(GPIO_PORT_P3, GPIO_PIN1 + GPIO_PIN2 + GPIO_PIN6 + GPIO_PIN7);
}
void initClock(void)
{
PMM_setVCore(PMM_CORE_LEVEL_3);
UCS_setExternalClockSource(XT1CLK_HZ, XT2CLK_HZ);
UCS_turnOnLFXT1(XT1DRIVE_0, XCAP_3);
UCS_initClockSignal(UCS_ACLK, UCS_XT1CLK_SELECT, UCS_CLOCK_DIVIDER_1);
//Configurate FLL
/*
UCS_initClockSignal(UCS_FLLREF, UCS_XT1CLK_SELECT, UCS_CLOCK_DIVIDER_1);
UCS_initFLL(DESIREDMCLK_KHZ, MCLKXT1CLKRATIO);
*/
myACLK = UCS_getACLK();
mySMCLK = UCS_getSMCLK();
myMCLK = UCS_getMCLK();
}
void initI2C(void)
{
USCI_B_I2C_initMasterParam I2cParam0 = {0,};
I2cParam0.selectClockSource = USCI_B_I2C_CLOCKSOURCE_SMCLK;
I2cParam0.i2cClk = UCS_getSMCLK();
I2cParam0.dataRate = USCI_B_I2C_SET_DATA_RATE_400KBPS;
USCI_B_I2C_initMaster(USCI_B0_BASE, &I2cParam0);
USCI_B_I2C_initSlave(USCI_B1_BASE, SLAVEADDRESS);
USCI_B_I2C_setSlaveAddress(USCI_B0_BASE, SLAVEADDRESS);
USCI_B_I2C_setMode(USCI_B0_BASE, USCI_B_I2C_TRANSMIT_MODE);
USCI_B_I2C_setMode(USCI_B1_BASE, USCI_B_I2C_RECEIVE_MODE);
USCI_B_I2C_enable(USCI_B0_BASE);
USCI_B_I2C_enable(USCI_B1_BASE);
USCI_B_I2C_clearInterrupt(USCI_B0_BASE, USCI_B_I2C_TRANSMIT_INTERRUPT);
USCI_B_I2C_clearInterrupt(USCI_B1_BASE, USCI_B_I2C_RECEIVE_INTERRUPT);
USCI_B_I2C_enableInterrupt(USCI_B0_BASE, USCI_B_I2C_TRANSMIT_INTERRUPT);
USCI_B_I2C_enableInterrupt(USCI_B1_BASE, USCI_B_I2C_RECEIVE_INTERRUPT);
}
I take a picture about I2C SCL and SDA at USCI_B_I2C_masterSendSingleByte. (Yello is SCL, Sky blue is SDA)

Where am i missing?
Thanks.