This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F6779: UART DMA problem with single transfer

Part Number: MSP430F6779

Good morning everybody!

I have a weird problem with my program on MSP430f6779. 

The problem is that when I have an empty while loop in the main file:

while{
}

it all works as expected. DMASZ counts down to zero and runs interrupt.

Everything changes when I put an additional for loop in the while loop.
while{
    for(i=0; i<3;i++){
        //do nothing
    }
}

Then the dma data transfer stops working.

Has anyone had a problem like this? 

//////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////////

Here you have my dma config: 

DMACTL0 = DMA0TSEL__USCIA1RX; // set DMA0 trigger to UCA1RXIFG 

__data20_write_long((uintptr_t) &DMA0SA, (uintptr_t) &UCA1RXBUF);
// Source block address
__data20_write_long((uintptr_t) &DMA0DA, (uintptr_t) &EXT_UART_buffer);

DMA0SZ = EXT_UART_BUFFER_MAX; //Ile danych ma przyjsc po uarcie
DMA0CTL = (0 << 12) | // 0: Single transfer, 4: Repeated single transfer ; Single transfer means the DMA will stop after filling the whole buffer
(3 << 10) | // Destination address is incremented
(0 << 8) | // Source address is unchanged
(1 << 7) | // Destination is byte
(1 << 6) | // Source is byte
(1 << 5) |
(0 << 4) | // DISABLE DMA // todo
(1 << 2) |
(1 << 0);

**Attention** This is a public forum