Part Number: MSP430FR6889
Hello,
I am uisng MSP430FR6889 and BMI160 Sensor. BMI160 has a 24-bit timer counter (BMI datasheet page 53).

I am trying to store this data but not sure if I am following the correct procedure.
I have written a I2C function that can access a the I2C slave and start reading from a address and reads till the specified amount of bytes.
I2C_Master_ReadReg(SLAVE_ADDR, 0x18, 3); //(slave address, Start register address, how many bytes to read)
Then I tried to store the data to a variable but MSP430 is showing me this worning: "64-D shift count is too large".
Here is that portion of the code:
uint32_t SENSORTIME;
uint8_t time_0 = 0;
uint16_t time_1 = 0;
uint32_t time_2 = 0;
time_0 = ReceiveBuffer[0];
time_1 = (uint16_t)(ReceiveBuffer[1] << 8);
time_2 = (uint32_t)(ReceiveBuffer[2] << 16);
SENSORTIME = (uint32_t)(time_2 | time_1 | time_0);
I think I know what I am doing wrong here. MSP430 is not a 32-bit MCU. Any suggestion on how to perform this operation?
Thank you.