Part Number: MSP430F2272
FET errors "UNKNOWN DEVICE" with datecodes: 18ATH2TG, 23A6RPTJ, ICA5R8TH
but works with 23AGRNTJ
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F2272
FET errors "UNKNOWN DEVICE" with datecodes: 18ATH2TG, 23A6RPTJ, ICA5R8TH
but works with 23AGRNTJ
Dennis,
the pull up resistor is a 47K and the cap to ground is 0.1u. there is a button switch to reset the device to ground.
this reset (not) line goes to two other devices as well: TE512 and a CP2102.
Hope this helps,
Let me know.
Thanks,
Bill:)
Hi William,
Not sure if it is a typo - bouble check your cap value. Should be 1 - 2.2nF, not 0.1uF
Dennis,
I figured it out. You were on the right track looking into the reset circuit. I have a schottky protection diode to prevent the reset line going negitive during power down. I had it in backward. My bad:( strange it didn't affect the TE512 or the CP2101.
Thanks for your help!
**Attention** This is a public forum