Part Number: MSP430FR5849
Hello,
When I check the electrical characteristics of the DCO in the data sheet,
I see that the DCO error is ±3.5% @ 1MHz.
Is this fixed for each individual device?
For example, ±1% for device A, ±2% for device B, and so on.
Or is there a DCO error per clock?
Or is this DCO error determined at each power supply startup?
Best regards,
DDdoor