Part Number: MSP430FG6426
Dear Team,
We see different conflicting information for this controller "MSP430FG6426IPZR" on the maximum operating frequency.
The product homepage shows 25Mhz https://www.ti.com/product/MSP430FG6426/part-details/MSP430FG6426IPZR
The datasheet says "High-frequency crystals up to 32 MHz (XT2)"
The same datasheet at "8.3 Recommended operating condition" section Page-28 says the maximum is 20Mhz
We need to run our product with the maximum clock as possible with this controller, Could you please help with the right information here on what is the maximum clock rate at which i can run this controller.
Note: Currently we use the internal oscillator with PLL to clock at 20Mhz, but we plan to use the external crystal on XT2 and try to use the maximum supported clock as possible.
Thanks
Surya