Part Number: MSP430F5310
What is the work flow until code reaches application after power on reset
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5310
What is the work flow until code reaches application after power on reset
Hi Nidheesh,
After a full reset or your power up ramp, the PMU will allow execution to begin. There is some low-level boot code that executes, and then the device checks for BSL signature and BSL protect value, (Shown in flowchart below - See section 1.2 of Creating a Custom Flash-Based Bootloader for more details on device BSL Startup Sequence). This tells the device whether or not to boot up in BSL mode. After those checks the device will normally run the C_INIT code, and then jump to the user application code (assuming BSL was not invoked).

Best Regards,
Brandon Fisher
**Attention** This is a public forum