Hi Team,
We have a usecase where we need to retain few bytes of data in the backup ram memory even during power down.
I have used a 3V battery in VBAT terminal (VBAK not used-Open) and XT1 32Khz crystal not mounted which mean i do not need the RTC feature at all.
In this case i do not see the backup memory retained during power down, and it always reads 0 after complete power down.
So my question is,
- is VBAK pin really required to have a supercap here although VBAT is supplied with a 3V constant battery backup ?
- Is XT1 required with 32khz and running the RTC module to have the backup memory active even during power down ?
this is how my register settings look like during runtime (if it helps)

Thanks
Surya