This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2332: ATEX Compliance Question

Part Number: MSP430G2332


Hello,

Can TI provide a written document for the following questions in order to use it as a certificate of conformance for the ATEX certification.

  1. The MSP430G2332IPW14R does not contain any voltage enhancement circuits?

OR

        2.The EEPROM charge pump voltage is not accessible from any external pins of the device?

AND/OR

        3.The maximum voltage from the charge pump is ?? V (or ? times the input voltage)

Regards,

  • Hi Matt,

    The MSP430G2332IPW14R does not contain any voltage enhancement circuits

    Not sure about what's kinds of voltage enhancement do you mean.

      2.The EEPROM charge pump voltage is not accessible from any external pins of the device?

    The MSP430G2332IPW14R do not has EEPROM, it just have flash and RAM.

    3.The maximum voltage from the charge pump is ?? V (or ? times the input voltage)

    Do you mean the charge pump for flash? If so there is no such voltage specification in the datasheet. 

**Attention** This is a public forum