Other Parts Discussed in Thread: TUSB3410
Hello all,
After playing with the launchpad, and loading it several times with different firmwares, it suddenly stopped being recognized by the PC.
When trying to debug using CCS, i get the following message:
Error initializing emulator:
No USB FET was found
The symptoms are exactly as in http://www.43oh.com/forum/viewtopic.php?f=8&t=822.
I tried to replace the cable and the uC chip itself, but it's still not get recognized (can't debug\download using CCS and the device is not even showing on the device manager).
The chip itself is working - the last downloaded firmware is still driving the launchpad leds and the top power led is on when the device is connected to the Pc, but I can't program it. I suspect the emulator is shorted or something like that.
Did anyone else got this message? Any solution?
Thanks.