Part Number: MSP430F5310
Hi,
From the below image which bootloader file support for MSP430F5310. Please clarify it.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP430F5310
Hi,
From the below image which bootloader file support for MSP430F5310. Please clarify it.
Hi Nidheesh,
I think you can refer to the demo
...\MSP430BSL_1_02_00_01\IAR_BSL_Source\IAR_v6_MSP430F543xA_TA_UART
Best regards
Gary
You can try this project
...\MSP430BSL_1_02_00_01\CCS_BSL_Source\CCS_v7_MSP430F543xA_TA_UART
No, I can't find such source code. But it should works with project I point to you.
Yes, I have mentioned before as below
...\MSP430BSL_1_02_00_01\IAR_BSL_Source\IAR_v6_MSP430F543xA_TA_UART
**Attention** This is a public forum