So I have the MSP430G2231 that comes with the launchpad series and it comes on an evaluation board that we can connect to the computer via USB cord and write code to it through CCS or IAR. My question is once the desired code is written onto the MSP430, and we disconnect the microprocessor from the eval board, how can we power/connect the processor to the rest of the circuit to make it work as programmed?
Specific concerns:
1) How to power it? Apply necessary voltage to VCC?
2) Do I need to add any external components? (Resistor, inductor, capacitors)?
Anything else I need to keep in mind?
Thanks for your help,
Kevin