Part Number: MSP430FR2476
Hi Team,
Good day! We need your assistance to clarify information with MSP430FR2476.
Our customer is considering using an external clock input to the MSP430FR2476 using XT1 input in bypass mode, i.e. supplying a square wave (from another MCU). We could not find any limits to the acceptable frequency range in the data sheet, only a "typical" figure of 32.768 kHz.
The other MCU can output a frequency with a period of 25 microseconds, equivalent to a frequency of 40 kHz. (This other MCU is crystal controlled, so this frequency can be considered "accurate".) Is this too fast for the MSP430FR2476?
In case there is some variation in the input clock frequency, e.g. +/- 1%, then the frequency could rise to 40.4 kHz. Is this too fast? What is the practical limit?
Thank you in advance for your support
Best regards,
Jonathan