Other Parts Discussed in Thread: MSP430G2231
Hi
I am having trouble reading analog values returned from the Ultrasonic Maxbotix LV-MaxSonar-EZ3 sensor on to ADC10 of my MSP430G2231 .
Basically when I use a voltimeter to read the sensor analog output without connect it to msp430 I have consistent results. The sensor scalling factor is VCC/512 thus, for my supply voltage (3.6v), we have ~7mv / inch. For example a value of 0.08v gives me a 11.42inches distance (~29cm).
For the same previous distance, when I plug in the analog pin on to INCH_3 of msp430 I'm getting the value of 186 from ADC10MEM, that converting to volts is equivalent to 0.65V (Volts = Nadc * VCC / 1023) . In fact I'm reading this value on voltimeter.
The strange thing is that increasing the distance the value remains basically the same. In the end I have only two readings 186 for short and 261 for long distances.
I am a newbie and don´t know what I'm doing wrong, I've tried to configure the ADC with all possible reference values whitout sucess.
I appreciate if someone can help me....
Here´s my code
//------------------------------------------------------------------------------------------------
#include <msp430g2231.h>
void ConfigureAdc(void);
void SampleDistance(void);
void main(void)
{
WDTCTL = WDTPW + WDTHOLD; // Stop WDT
ConfigureAdc();
for (;;)
{
SampleDistance();
}
}
void ConfigureAdc(void)
{
ADC10CTL0 = ADC10SHT_2 + ADC10ON + ADC10IE;
ADC10CTL1 = INCH_3 + SHS_0 + ADC10SSEL_0;
ADC10AE0 |= 0x08 ;
}
void SampleDistance(void)
{
ADC10CTL0 |= ENC + ADC10SC;
__bis_SR_register(CPUOFF + GIE);
adc = ADC10MEM;
}
// ADC10 interrupt service routine
#pragma vector=ADC10_VECTOR
__interrupt void ADC10_ISR (void)
{
__bic_SR_register_on_exit(CPUOFF);
}