Hello
I wish to program a segment of the information flash in the MSP430F2013 using the beeprog2 programmer from ELNEC without changing the content of the remainder of the flash.
When setting the programmer to use standard JTAG it has an option to program information memory without touching the DCO constants and the program flash however when changing to spy-by-wire this option is removed.
The programming should be used during production for writing calibration constants to the information flash and should use spy-by-wire due to reduction in wiring, which will enable the use of existing tools.
If i have understood correctly there should be no difference between the spy-by-wire and the full JTAG interface except for the speed. This does however not seem to be the case when using the beeprog2 programmer and software. Is this because they have not implementet the feature or is there a limitation in the spy-by-wire interface.
Frank Hansen