Hi Friends.
I am working on 4-wire RTD(PT100). I want to use MSP430 including Delta-Sigma ADC. Which one can i use? What is yours offers?
Thanks...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Friends.
I am working on 4-wire RTD(PT100). I want to use MSP430 including Delta-Sigma ADC. Which one can i use? What is yours offers?
Thanks...
Alls MSP with an SD16 module :)omeraygor said:I want to use MSP430 including Delta-Sigma ADC. Which one can i use?
For 4-wire PTC usage, you usually want to put an impedance transducer between the PTC and the MSP, but the PT100 has a low enough impedance so that the comparably low input impedance of the SD16 doesn't count.
However, getting a voltage high enough to give a significant signal on the SD16 (even with an input amplification of 32, as some SD16 offer), will require a relatively large current through the PT100, which in turn will influence the sensor readings. (several 100µA give several µW internal heating, without amplification, this will enlarge to some mW!)
So I suggest using an external OpAmp that amplifies teh PT100 voltage by a suitable factor (e.g. 100). It will be more precise than the internal amplification of the SD16 too and give a better SNR.
Hi Micheal.
Nİce to meet you again.
I looked into some ICs that include Sigma - Delta ADC and suitable to measure RTD. These is AD7714 and AD7730.
These have opamp and Sigma - Delta ADC block.

What about your opinion?
In the circuit above, teh OpAmps are used as a (not 100% but nearly) constant current source (the current changes with the resistance of RTD, but with a factor of 200 less). So the voltage over the RTD changes linear with the temperature. Ref- is Vin and Ref+ is Vin +2V. Power over the RTD is 1µW
However, the voltage over the RTD is only 10mV, which is really not much. So I would still suggest an external amplification by a factor 100.
**Attention** This is a public forum