Other Parts Discussed in Thread: TM4C123GH6PZ
Hi,
I currently have several designs that use the MSP432P401RIPZ. This is a 100-pin LQFP package with 256 kB Flash, 64 kB SRAM, and 48 MHz max operating frequency. This MCU has been discontinued, so I'm looking for a replacement that is close in specifications and size (100-pin LQFP, 14 mm x 14 mm). Are there any recommendations? A specific TM4C or drop down (and optimize) to a MSP430 with 25 MHz clock?
Thanks.