This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error[e77]: error while using MSP430f5438

Other Parts Discussed in Thread: MSP430F5438

Hi,

  i am using msp430f5438  with a USB fet430UIF emulator. I am using IAR Workbench Evaluation Version.. i just started with the basic led flash code..but the code is giving me two error. Plzz help me out in this. Thanks in advance

My code is :-


#include "msp430.h"
;-------------------------------------------------------------------------------
            ORG     0FC00h                  ; Progam Start (1K Flash device)
;-------------------------------------------------------------------------------
RESET           mov.w   #0150h,SP                                                             ; Set stackpointer (128B RAM device)
StopWDT       mov.w   #WDTPW+WDTHOLD,&WDTCTL                     ; Stop watchdog timer
SetupP1         bis.b   #001h,&P1DIR                       ; Set P1.0 to output direction
                                                                                       ;
Mainloop       XOR.b   #001h,&P1OUT                    ; Toggle P1.0
Wait                MOV.w   #050000,R15                       ; Delay to R15
L1                    DEC.w   R15                                       ; Decrement R15
                        JNZ     L1                                              ; Delay over?
                       JMP     Mainloop                                   ; Again
                                            ;
;-------------------------------------------------------------------------------
;           Interrupt Vectors
;-------------------------------------------------------------------------------
            ORG     0FFFEh                  ; MSP430 RESET Vector
            DW      RESET                   ;
            END

It is giving me a error:-

Error[e77]: The absolute segment on the address fffe-ffff in the module Flash_led (E:\MSP\Workspace\Debug\Obj\Flash_led.r43) overlaps the absolute 
segment on the address fffe-ffff in the module main (E:\MSP\Workspace\Debug\Obj\asm.r43)

Error while running Linker

 

**Attention** This is a public forum