As title, Can I bypass the limit of 9600bps of the ez430-RF2500 USB debugger and have a higher data rate please?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
As title, Can I bypass the limit of 9600bps of the ez430-RF2500 USB debugger and have a higher data rate please?
Sure: make your own interface hardware.
Connect the MSp with a level shifter such as the MAX232 or similar and connect it to a serial port (or an USB to serial adapter). Then you'll have no problems going up to 115200 and more.
With the provided hardware: no.
See my answer in this other (even older) thread which you revived with the same question.Kai Liu101519 said:With internal DCO clock? Is it possible?
**Attention** This is a public forum