Part Number: MSP430FR6922
Other Parts Discussed in Thread: MSP-FET
Hello,
I want to run the timer @1000 hz freq in continuous mode and I am doing some comparisons in timer interrupt and take AD7190 adc data values. I am transmitting this adc's values in seperate while loop. When MSP-FET is connected timer interrupt is working fine and correct data transmit to to rpi. But, after flash the cde in MCU and disconnected the emulator from MCU timer adc's value are not change. in while loop data transmit to rpi i.e. adc values. but those values are constant its not change.
What is the issue. I have attached code for your ref.
#include "common.h"
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // Stop WDT
variable_Set_zero();
pin_init();
dev_init_16M(); // Microcontroller set on 16MHz
RPI_UART();
Timer();
SPI_INT(); // SPI initialization
AD7190_register_read();
__enable_interrupt(); // Re-enable all interrupts
__bis_SR_register(GIE); // Enter LPM3, interrupts enabled
while (1)
{
if(DelayStart==1) // For sample 1 send LC data after every 1 sec to tare the LC readings
{
// (DCO=MCLK=16MHZ )so,
// Count/MCLK freq=Time
// 16000000/16MHz=1sec
__delay_cycles(16000000); // delay calculate on 16 MHz
AD7190_CH1_setup();
//while(!((P1IN&BIT7)==0)){} // Wait until data ready
CurrentLCValue=ReadData(); // Read load cell data
CurrentLCValue1=CurrentLCValue&0x7FFF;
LongtoInt.LongData=CurrentLCValue; // Split 3 byte data into single byte
giTransmitBuffer[0]=LongtoInt.ByteSplit[1];
giTransmitBuffer[1]=LongtoInt.ByteSplit[0];
giTransmitBuffer[2]=0x00;
for(i=0;i<3;i++) // Upto array from start to CRC lenth
{
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF = giTransmitBuffer[i];
}
}
if (DataStart==1)
{
__delay_cycles(16000);
LongtoInt.LongData=CurrentLCValue;//LoadCellData is in 16 bit first 2 byte;
giTransmitBuffer[0]=LongtoInt.ByteSplit[1];
giTransmitBuffer[1]=LongtoInt.ByteSplit[0];
giTransmitBuffer[2]=0x00;
for(i=0;i<3;i++) // upto array from start to CRC lenth
{
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF =giTransmitBuffer[i];
}
}
/*******************************Test Stop if overload+***************************/
if (teststop==1)
{
//timer stop
TA0CCTL0 &= ~CCIE;
RTCCTL0_L &= ~RTCTEVIE; //rtc disabled
// relay off
P7OUT &=~BIT0;
teststop=0;
}
}
}
void send_start_command(void)
{
giTransmitBuffer[0]=0xAA;
giTransmitBuffer[1]=0xBB;
giTransmitBuffer[2]=0xCC;
giTransmitBuffer[3]=0xDD;
giTransmitBuffer[4]=0xEE;
giTransmitBuffer[5]=0xFF;
for(i=0;i<6;i++) // Upto array from start to CRC lenth
{
while(!(UCA0IFG&UCTXIFG));
UCA0TXBUF = giTransmitBuffer[i];
}
}/*
* Timer.c
*
* Created on: 09-Sep-2022
* Author: Admin
*/
#include "common.h"
void Timer(void)
{
//Timer Period in Seconds = DIV x (TACCR0 + 1)/Input Clock in Hz
//freq=1/timer period
//TA0CCR0=(Input Clock in Hz/DIV*Freq)-1;
//TA0CCTL0 = CCIE; // TACCR0 interrupt enabled
TA0CCR0 = 4000; //(4MHz/4000=1000 Hz)
TA0CTL = TASSEL__SMCLK | MC__CONTINUOUS; // SMCLK, continuous mode
}
// Timer0_A0 interrupt service routine
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = TIMER0_A0_VECTOR
__interrupt void TIMER0_A0_ISR (void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(TIMER0_A0_VECTOR))) TIMER0_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
if(Data==1)
{
send_start_command();
AD7190_CH1_setup();
//while(!((P1IN&BIT7)==0)){} // Wait until data ready
CurrentLCValue=ReadData(); // Read load cell data
DataStart=1;
}
Data=0;
AD7190_CH1_setup();
//while(!((P1IN&BIT7)==0)){} // Wait until data ready
CurrentLCValue=ReadData(); // Read load cell data
CurrentLCValue3=CurrentLCValue&0x7FFF;
if(CurrentLCValue3>=0x1F59) // if 9F5961=10443105=9.567mV=675 psi (90 percent of 10.63 mV means 750 psi) is reached test stop
//9F59&7FFF=0x1F59
{
Error[0]=0x10;
Error[1]=0x10;
Error[2]=0xAA;
teststop=1;
}
TA0CCR0 += 4000; // Add Offset to TA0CCR0
}