This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR5043: BSL ACK error

Part Number: MSP430FR5043
Other Parts Discussed in Thread: MSP430FR6989

Hi, 

I'm currently working on MSP430FR5043.

I need to upload my program using UART bootloader for example : LED blinking. (using UART bridge CP210x)

Here the issue is I'm getting error ack.

For script file I used  /ScriptExampleWindows/FRxx_uart/script_FRxx_uart.txt file in BSl_scripter package

the default script is for MSP430FR6989. Considering the controller I'm using is MSP430FRxx family

the only thing I changed is COM port which is COM3 and program file ledblink.txt.

Below is the response I'm getting.

What would be the issue here connected pins 

TX RX 

DTR - RST/NMI

RTS - TEST

 

Thanks in advance.

**Attention** This is a public forum