This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F4152: MSP430 Design and Manufacturing Expert needed

Part Number: MSP430F4152

Dear all, 

I would like to include the MSP430 in my doctoral thesis. For that I need the support of an MSP430 Design and Manufacturing Expert. Can you help me? Thanks! 

Best regards

Jaime 

  • Hello,

    If you have specific questions about the device and how to use it, we can answer them here. That being said, I see your tags are related to radiation and space, so my assumption here is your questions relate to that. If so, your chosen MSP430F4152 is only rated for industrial environments and may not perform correctly or to datasheet specifications when subjugated to radiation or "space" environments. 

    We do have an MCU that would be more appropriate for that type of environment. See MSP430FR5969-SP 

  • Hello Jace, 

    Thank you for your answer. 

    I would like to investigate the radiation effects on MSP430 COTS. For that I will achieve radiation tests and the DUT's should be MSP430 devices from wafers which manufacturing process has small differences. I will need then the mentioned devices and details about the manufacturing process. As you can see is not a standard use of MSP430 COTS. At the end of my study I will share the results with TI.

    I can give for sure more details about the project later.

    Best regards 

    Jaime 

  • Dear Jace,

    Can you support me in this issue?

    Best regards

    Jaime

  • Hello Jamie,

    This is not something we can support at this time. Please see our space grade part mentioned earlier and associated documentation around that. 

**Attention** This is a public forum