Part Number: MSP430FR5969
Hi,
I am using two counter modules,(TIMERA1, and TIMERA2) to count external pulses, To test the module I am providing input through external Function Generation and there is also an internal pulse generator that will provide input at a 5 min interval when these two signal meet the sometimes the module resets after 5 minutes interval in an irregular manner.
If the Function generator input is not provided it works without resetting for more than hours, how could I stop reset of the microcontroller?
but in the Debug mode the reset scenario does not take place, how could I implement it during normal operation?