Dealing with lots of problems at once, I plunged in the 14-pin MSP-FET430UIF to the target board while both the target board and the FET were hot (powered up – BAD ME!)
This corrupted the firmware on the MSP-FET430UIF. CCS gave me the error message when attempting to debug -- the security fuse was blown.
Down load the following software, read the user guide.
http://www.elprotronic.com/files/FET-Pro430-Lite-Setup.zip
I did the following: Setup Menu > Connection/Device Reset > Select the proper type of port used.
Tools > MSP-FET430UIF Firmware Downloader > Re-flash the firmware
Back in the saddle again :)