Part Number: MSP430-FLASHER
Other Parts Discussed in Thread: MSP-FLASHER
I have two USB MSP-FET430UIF JTAG pods that are used in programming certain hardware.
Recently I started seeing one of our automated tests fail and traced the issue back to one of the MSP430 pods.
I have the two on COM8 and COM22. The failing pod is on COM8 and the one that work is on COM22. If I change the pod on COM22 to COM8, our automated test passes. Then I can move it back to COM22 for test number 2.
This led me to believe a bad pod, so I ordered two replacements. However I get the same error on both new pods!
"* Driver : closed (Internal error)"
However, switching back the same working model MSP430UIF from COM22 to COM8 using the SAME batch file. Any troubleshooting help is appreciated!