This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F5437A: MSP4305437A

Part Number: MSP430F5437A
Other Parts Discussed in Thread: MSP430F5437,

Hi,

I have this TI microcontroller with part number "MSP4305437A Rev F" on it.

But when I connect it to the flashpro via JTAG and do an AUTO PROG., I see the following error:

I tried changing the Microcontroller type to MSP430F5437 and then I don't see the above error.

I tried referring to the datasheet of MSP430F5437 and I could see that it is Rev-F. 

If it is actually MSP4305437 then can you let me know why the part number on it is mentioned as MSP4305437A?

Regards

Lakshmi

**Attention** This is a public forum