Hello, I have been working with the example of an ultrasonic sensor, I have read the api manual and I would like to know if it is possible to make the code take the data from it and transmit it via uart?.
That is, I would like to see if I can obtain the data of the number of liters that pass through the pipe and can be sent via a uart to be read by another device?
From what I could understand from the api manual, it is possible to make slight modifications such as establishing default calibration parameters.
And one part talks about how we as programmers can get that data, and do our calculations, but where in the package can that function be added?
I will leave the manual here attached