Part Number: MSP430F1611
Dear TI expert,
Now i am designing a BMS with use MSP430F1611 UART1 communication with one host, the host use modbus protocol, only two device, so i use the asynchronous communication formats, the idle-line format is used for the protocol.
the serial port configuration as follow: baud rate is 9600, data bit is 8, no parity bit, two stop bit
the modbus protocol like this:0x01 0x03 addresshi addresslo numhi numlo crc16lo crc16hi
the uart1 configure as follow:
void VMU_UART_INIT_9600 (void)
{
BCSCTL1 |= XTS; //high frequency mode
UCTL1 |= SWRST; // Initial uart
UTCTL1 = SSEL0; // ACLk(32768), default charactor, not address
UBR01 = 0xC0; //Baud rate :9600 ACLK: 1843200/192 = 9600
UBR11 = 0x00;
UMCTL1 = 0x00;
UCTL1 |= CHAR + SPB; //8 bit, no parity check, two stop bits
P3SEL |= 0xc0; //P3.7 RX,P3.6 TX
P3DIR |= 0x40;
P5DIR |= BIT4; // Transceiver DE,RE enable
P5OUT &= ~BIT4; // DE=0, R/E/=0 RX is default state, not TX
UCTL1 &= ~SWRST; // start uart
ME2 = UTXE1 + URXE1; // uart1 tx and rx module enable
IE2 |= URXIE1;
}
ISR receive as follows:
Since I can't judge the start and end of a packet, my idea is to wait for the next byte to be set to URXIFG and read the receive buffer register when the first byte received is 0x01, 1200 is timeout value
#pragma vector=UART1RX_VECTOR
__interrupt void RX_VMU_BYTE (void)
{
U8 i;
U16 time;
VMURS485Buf[0]=RXBUF1;
if (VMURS485Buf[0] == 0x01)
{
for (time =0; time <1200 && !(IFG2&URXIFG1); time++)
if (time < 1200)
VMURS485Buf[1]= RXBUF1;
if (VMURS485Buf[1] == 0x03)
{
for (i = 2; i < 8; i++)
{
for (time =0; time <1200 && !(IFG2&URXIFG1); time++)
if (time < 1200)
VMURS485Buf[i] = RXBUF1;
}
}
UART_Response(VMURS485Buf);
}
}
when i use the serialport software send command 0x01 0x03 0x00 0x01 0x00 0x06 crclo crchi
but VMURS485Buf[1]= RXBUF1; is 0x01 not 0x03
the value 1200 is timeout