Hi Team,
Here's an issue from the customer may need your help:
When working normally, the comparator outputs a square wave.
The watchdog will reset the MCU after 1 second if the comparator output does not change. Use an oscilloscope to see that the watchdog keeps resetting. The comparator will work normally after hardware reset(short reset pin to ground).
The source of interference is caused by another circuit board starting the motor.
The probability of the problem is one in a few tenths to one in a few hundredths.
How to resolve this issue?
Thanks & Regards,
Yale Li