Part Number: MSP430F5529
Other Parts Discussed in Thread: MSP-EXP430F5529LP
Hello,
I am having troubles making the interrupt to work. I want the red led to toggle every 1s.
After 1 toggle the code stays trapped in SFR trap. In debug I see GIE is cleared. In normal mode, after a reset, it toggles once or twice (randomly) and then nothing happens.
What am I missing?
#include <msp430.h>
#include <lcd.h>
#include <stdlib.h>
#include <stdio.h>
#define RED_LED_ON() P1OUT |= BIT0
#define RED_LED_OFF() P1OUT &= ~BIT0
#define RED_LED_TOGGLE() P1OUT ^= BIT0
void SetupUCS(void);
void SetupTimers(void);
void main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
P1DIR |= BIT0; // configure P1.0 as output
P4DIR |= BIT7; // configure P4.7 as output
SetupUCS();
SetupTimers();
while(1)
{
GREEN_LED_TOGGLE();
__bis_SR_register(LPM0_bits + GIE);
__no_operation();
}
}
void SetupUCS(void)
{
//set clock source to XT1
P5SEL |= BIT2+BIT3+BIT4+BIT5; // Port PINs function select XT1 32768Hz and XT2 4MHz
UCSCTL6 &= ~(XT1OFF); // XT1 On
UCSCTL6 &= ~(XT2OFF); // XT2 On
//UCSCTL6 |= XCAP_3; // Internal load cap. necesar? exista 2 condensatori pe placa!
// Loop until XT1,XT2 & DCO fault flag is cleared
do
{
UCSCTL7 &= ~(XT2OFFG + XT1LFOFFG + DCOFFG); // Clear XT2,XT1,DCO fault flags
SFRIFG1 &= ~OFIFG; // Clear fault flags
}
while (SFRIFG1 & OFIFG); // Test oscillator fault flag
UCSCTL4 &= ~(SELA0 + SELA1 + SELA2); // ACLK source set to XT1CLK
UCSCTL4 &= ~ SELS1; // SMCLK source set to XT2CLK
UCSCTL4 |= SELS0 + SELS2;
UCSCTL4 &= ~ SELM1; // MCLK source set to XT2CLK
UCSCTL4 |= SELM0 + SELM2;
UCSCTL5 &= ~ DIVA1; // divide ACLK by 32
UCSCTL5 |= DIVA0 + DIVA2;
UCSCTL5 &= ~ (DIVS0 + DIVS2); // divide SCLK by 4
UCSCTL5 |= DIVS1;
}
void SetupTimers(void)
{
TA0CCTL0 |= CCIE; // CCR0 interrupt enabled
TA0CCR0 = 1023; // get an interrupt every 1s
TA0CTL |= TASSEL0 + MC0 + TAIE + TACLR; // ACLK, up-mode, TA0 clear, Enable TA0 interrupts
}
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector = TIMER0_A0_VECTOR
__interrupt void TIMER0_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__((interrupt(TIMER0_A0_VECTOR))) TIMER0_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
/* Any access, read or write, of the TA0IV register automatically resets the
highest "pending" interrupt flag. */
RED_LED_TOGGLE(); //any timer 0 interrupt. for debug
switch( __even_in_range(TA0IV,14) )
{
case 0: break; // No interrupt
case 2: // CCR1
RED_LED_TOGGLE();
break;
case 4: break;
case 6: break;
case 8: break;
case 10: break;
case 12: break;
case 14: break;
default: break;
}
}
Thank you,
Catalin