Other Parts Discussed in Thread: TM4C1290NCZAD
Hi team,
I want to use msp430 launchpad and tm4c1290nczad launchpad for spi communication.
Simplly speaking, i use msp430 send some data ,and tm4c will receive these data.
but now,I have two question .
I burned the test codes for the two boards separately . and connect SIMO,SOMI,CLK,CS,Signals.
On CCS ,I have to click the red cycle to run the code.I can't click the run button for both codes at the same time.

(1) How should I exit the debug mode and let the system run automatically .?
(2) How to debug spi communication between two boards , is there any routine?
I look forward to your reply
Thank you