Can I use the ADC’s or the DACS at 33 kHz.
- I need to digitize 33 kHz sine wave
- I need to generate a 33 kHz sine wave, with filter
Do any internal filters limit frequency performance?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can I use the ADC’s or the DACS at 33 kHz.
Do any internal filters limit frequency performance?
Hi,
Based on the datasheet, you can use the ADC and DAC at 33kHz.
The data in the chapter 8.8.13.5 has already considered the influence of filter.
Best regards,
Cash Hao
Does the ADC have an anti-aliasing filter? Where does the clock for the ADC come from? Where does the clock for the DAC come from?
Regards,
Chris
Hey Chris,
To clarify here, the fastest signal this device, with its CTSD16 ADC, will be able to sample is 32kHz. This is due to the oversampling ratio (OSR) that is built into the CTSD16. F_S = F_M/OSR = 1.024MHz/32 = 32kHz. OSR=32 is the lowest OSR available for this device.
**Attention** This is a public forum