Other Parts Discussed in Thread: UNIFLASH
Hello,
I am working with the evaluation board EVM430FR6047.
First day working with it, I installed drivers and USS Design Center SW and all worked proprerly.
Suddently at one moment all stop to work, and I got Error Code 255 "Unknown error". I tried to reinstall, connect and disconnet, install MSPWare and so on. Nothing worked
So I decided to re-flash the Firmware by installing uniflash 8.1.1 and reload the Demo Image "MSP430FR6047EVM_USS_Water_Demo_LPM_02_20_00_04.txt". Flashing gone well.
Now I get a different error code 126 "No signal detected in up or downstream channel", and the connection status gives "HID Bridge connected - waiting for device". The LED3 in blinking red.
Strangely if I try to capture the signal through "ADC Capture" I have some proper signal but I cannot changed any parameter because the "Request Update" button is greyed.
I am working with Windows 10 Enterprise (20H2), the EVM430FR6047 board and a connected pipe where transducers are properly connected to the board.