Dear Sir or Madam,
I have recently ordered the board "EVM430-FR6047" via digikey. I would like to connect an ultrasonic flowmeter from Audiowell to this board. The flow meter has the part number: HS0014. Below you can find my circuit:
Now to the USS software. I get the error "No signal detected in up and downstream channel" with the following settings (see last picture). However, if I turn the GUI Based Gain Control to Maxium (30.8), the LED3 on the board goes off and only shows up now and then with the error "dToF - Correlation overrun error". The signal in the ADC capture looks like this:
Furthermore I could not receive better signals in the ADC Capturing with low "GUI Based Gain Control". My assumption is that I must have plugged something wrong or the sensor is possibly broken, because it does not send any signals.
I hope you can help me.
Thanks a lot in advance.
With kind regards
Jérôme Noglinski