Part Number: MSP430FR2475
Hello,
I have a few questions about the I2C driver code in the resource explorer for MSP430FRxxx.
1. In the MSP430 example code for the I2C driver, I found a function called 'CopyArray'
```
void CopyArray(uint8_t *source, uint8_t *dest, uint8_t count)
{
uint8_t copyIndex = 0;
for ( copyIndex = 0; copyIndex < count; copyIndex++ ) {
dest[copyIndex] = source[copyIndex];
}
}
```
there doesn't seem to be anything special about the source or destination buffer here. Is there any reason to use CopyArray over memcpy, which allows one to directly copy source buffer to destination buffer without use of a loop?
2. In the I2C ISR, there are some global variables used to keep track of Rx and Tx count, namely, `RXByteCtr` and `TXByteCtr`. These globals are modified both in the ISR and outside of the ISR.
In the `I2C_Master_ReadReg` function, both of these variables are modified (RxByteCtr set to count, TxByteCtr set to 0) before disabling Rx interrupt:
```
RXByteCtr = count;
TXByteCtr = 0;
ReceiveIndex = 0;
TransmitIndex = 0;
/* Initialize slave address and interrupts */
UCB1I2CSA = dev_addr;
UCB1IFG &= ~(UCTXIFG + UCRXIFG); // Clear any pending interrupts
UCB1IE &= ~UCRXIE; // Disable RX interrupt
```
and similarly in `I2C_Master_WriteReg`. Won't this cause problems where the Rx/TxByteCtr might get modified after being set, since the interrupt isn't disabled before modifying/reading the value? Also, should the variables not be declared as volatile and static to this I2C driver file?
Warm regards,
Samyukta