This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430I2041: DCO accuracy and TCR

Part Number: MSP430I2041

Hi,

According to datasheet, DCO temperature drift with an external resistor with 50ppm TCR is +/-0.29%.


My customer is asking if a resistor with 25ppm TCR is used how the value is changed.
Do we have such data?

Thanks and regards,
Koichiro Tashiro

  • Hello,

    We do not have additional data outside the specifications shown in the datasheet here for a tighter tolerance external resistor. My intuition says you may get some slightly better accuracy, but would be diminishing returns from what is stated in the datasheet. 

**Attention** This is a public forum