Part Number: MSP430F5529
Hi Team,
We received the following inquiries from our customer.
I would like to use the MSP430F5529 in an application to test different voltage rails via pogo pins. I will be utilizing the Vref for analog reference and analog switches to input into the 3 of ADC input pins. My application should output data to the serial console over USB. My questions are as follows.
1. I understand the MSP430 has USB built in so I can directly connect the USB 2.0 signals to the MCU (with proper ESD protection). Do I need any other components to enable USB operation such as an external clock. I understand there is an integrated clock in the MSP but would this application benefit from and external clock? Will an external clock/crystal reduce current drawn from the MSP? From the eval board schematic, I see there are two external crystals being used, which makes me question if it a requirement in this application.
2. Do I need to configure the MSP to boot with USB. If plug the USB signals to MSP will it appear as a COM device and ready to be programmed? I understand the BSL is preprogrammed on the device, but the datasheet also mentioned is it protected by a user defined password as well? Can you explain further on how I can get around the password and program the board with my code.
3. In the datasheet section 8.3, footnote 2 suggested the DVCC and AVCC should be from the same source. My current design has the analog and digital supplies (3.3V) from different supply components so the analog circuity is not susceptible to noise or spikes. Will that suffice? Should I opt into keeping the supplies the same and utilize a pi filter for the core and analog inputs.
Regards,
Danilo