I have to believe this has been asked before but believe it or not, I cannot find a question for this issue.
I am running CC on mac os Venture 13.1. When I compile, I get errors for (primarily) the following:
"Description Resource Path Location Type
Content is not allowed in prolog. in file /Volumes/T7-MBx86/projects/MSP4305994/poop/targetConfigs/._MSP430FR5994.ccxml ._MSP430FR5994.ccxml /poop/targetConfigs line 1 Problem"
So, it astounds me that CC is even paying attention fo the classic max os "._xxx" files. I am further astounded that there is no setting to view and ignore these files within CC. I would have expected to see something in the README.txt file when I installed CC on the mac. I initially tried using Parallels with Windows 10, but I am using an older launch pad (MSPfr5994) which, I know, has issues with the USB, or so I thought.
Anyway, not to sound cynical, just wondering what others do with the unrelated (to CC) "dot files"?
Thanks,
Dave Comer