Part Number: MSP430FR4133
Other Parts Discussed in Thread: MSP430G2553
Im trying to map code from an existing library I found so that I can drive a ws2812b LED strip. I found the library here https://github.com/mjmeli/MSP430-NeoPixel-WS2812-Library. Ive made an attempt at mapping it for my specific part but the code still does not seem to work. There are 3 small sections that I need to change for my specific part and here are my attempts. The 3 blocks of code include the original code as well as my equivalent code. I need help with identifying a problem or some tips on how to map code from one MSP to another as I have no experience with doing so.
The first section is needed to configure the UCB0SIMO as the SPI Output
// ORIGINAL
#define OUTPUT_PIN (0x80) // Set to whatever UCB0SIMO is on your processor (Px.7 here)
P1SEL |= OUTPUT_PIN; // configure output pin as SPI output
P1SEL2 |= OUTPUT_PIN;
//My equivalent code
P5SEL0 |= BIT2; // configure output pin as SPI output
The second is checking the UCB interrupt flags. This is where I think the problem may be coming from? On the datasheet for my part this is in the data sheet: UCB0RXIFG, UCB0TXIFG (SPI mode) but when I use them I get an undefined error.
// Original Code while (!(IFG2 & UCB0TXIFG)) ; // wait to transmit // My equivalent code while (!(SFRIFG1 & UCTXIFG)) ; // wait to transmit
And the 3rd section is initialising a 16 MHz clock
//Original Code
if (CALBC1_16MHZ==0xFF) // If calibration constant erased
{
while(1); // do not load, trap CPU!!
}
// configure clock to 16 MHz
BCSCTL1 = CALBC1_16MHZ; // DCO = 16 MHz
DCOCTL = CALDCO_16MHZ;
// My equivalent code
void initClockTo16MHz()
{
// Configure one FRAM waitstate as required by the device datasheet for MCLK
// operation beyond 8MHz _before_ configuring the clock system.
FRCTL0 = FRCTLPW | NWAITS_1;
__bis_SR_register(SCG0); // disable FLL
CSCTL3 |= SELREF__REFOCLK; // Set REFO as FLL reference source
CSCTL0 = 0; // clear DCO and MOD registers
CSCTL1 &= ~(DCORSEL_7); // Clear DCO frequency select bits first
CSCTL1 |= DCORSEL_5; // Set DCO = 16MHz
CSCTL2 = FLLD_0 + 487; // set to fDCOCLKDIV = (FLLN + 1)*(fFLLREFCLK/n)
// = (487 + 1)*(32.768 kHz/1)
// = 16 MHz
__delay_cycles(3);
__bic_SR_register(SCG0); // enable FLL
while(CSCTL7 & (FLLUNLOCK0 | FLLUNLOCK1)); // FLL locked
CSCTL4 = SELMS__DCOCLKDIV | SELA__REFOCLK;
}