Part Number: MSPM0
Hello,
I've a problem regarding setting TIMG0 registers in MSPM0 controller.
If I try to set any register to any value, nothing works. Is the TIMG0 register protected or something like that?
I figured out, that also other timer register such as TIMA0 or any other register with Peripheralregion can't be written to some value.
Only the SYSCTL, FLASHCTL, SysTick registers can be set to any value, which are not part of the Peripheralregion.
So I think the problem has to be with the Peripheralregion.
Can you help me to write to registers which are part of Peripheralregion?
Thank you!
Best regards
Felix