This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2422: Endurance of FRAM

Part Number: MSP430FR2422


Hi,

I am using a variable called timestamp to keep track of time in seconds. This variable has to be updated every second. Can I use #pragma PERSISTENT and store the value of the variable in FRAM. 

If yes, how many write cycles is guaranteed.

  • >> Can I use #pragma PERSISTENT and store the value of the variable in FRAM. 

    Yes. you can

    >> If yes, how many write cycles is guaranteed.

    according to data sheet, Read and write endurance of FRAM is 1015 cycles and the Data retention duration is 10 years at 85°C

    this endurance cycle include both read and write cycle. So, I can't give an exact number, but it's durable.

    Thanks!

**Attention** This is a public forum