This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430F2012: Modeling IO in simulation

Part Number: MSP430F2012

I am simulating several parts of an analog circuit that interfaces with an MSP430G2012 using the integrated simulator in Altium Designer. I want to include an output from the analog circuit that is used as an input into the microcontroller's 10-bit ADC, as well as GPIO microcontroller output that drives the gate of a  MOSFET. Can you provide any recommendations on modeling the ADC input or GPIO output?

Mark McGahan

mmcgahan@ced.us.com

**Attention** This is a public forum