Part Number: MSP430F5507
Hello,
I would like to ask Msp430 USB BSL firmware update.
We use the Msp430F5507 on our custom board.
When the OS of PC was "Windows 7", I could do USB BSL firmware
update without problems, by using Msp430 Usb Bsl
and the Visual Studio project for it.
(When I pressed the reset-button of Msp430 MCU,the PC detected
Usb Bsl Device.)
But,now, it could not be done on Windows10.
When I pressed the reset-button of Msp430 MCU , the windows10 PC
doesn't recognize Msp430 USB Bsl device.
What should I do to solve it ?
The version of Msp430 USB Bsl is 1.00.12 (IAR).
Regards,
Hiroyasu Matsubara