This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2433: MSP430FR2433IRGER

Part Number: MSP430FR2433


Hi,

Let me provide some background on the problem:

  • Vdd is 3.1V
  • To save power, the microcontroller (µC) is put in sleep mode.
  • To wake it up, we change the state of a GPIO pin using an external signal, which we'll call S_ext.
  • Sometimes we detect that the voltage of S_ext is greater than Vcc+0.3.

According to the datasheet, the amplitude of the signal going into the GPIO should not be greater than Vcc+0.3V. However, our product still seems to be working.

I have some questions:

  • If the condition Vcc+0.3 is not met, can the µC still be functional? What are the risks?
  • Is the only risk that the pin's ESD protection might be broken? Our product is resin-coated to avoid ESD issues. Is that why it's still working after applying a signal greater than Vcc+0.3V to the pin?
  • What will happen if the voltage applied to the pin is more than 4.1V?

Thank you in advance 

Best regards 

Liang

**Attention** This is a public forum