This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430G2230: Store data in flash when updating firmware

Part Number: MSP430G2230

Hello, 

I am planning to use part of the flash memory in MSP430G2230 as non-volatile memory to store some data. I am wondering if I can directly put the data in the flash when uploading the firmware onto the chip, so I do not need to write function to store data in flash.

The reason why I need this is because I need to write 640 bytes of data into flash while RAM of MSP540G2230 is only 128 bytes, so I am not able to write all the data I need into flash at once. 

Thanks in advance. 

**Attention** This is a public forum