Part Number: MSP430FR6043
Hi.
Two questions on the algorithms:
1. Can we have some sort of an API for the closed-sourse algorithms library? We have developed our own set of algorithms for both dToF and absToF computation but there is quite a lot of overlap with the functions already in the USS library and I can see that they are very well-optimized as they use very little power. Ideally some sort of access to the cross-correlation function (CCF) computation function (whichever one it is out of USS_corr, USS_corr3, USS_corrN) and the peak interpolation.
2. If not -- is it possible to extract the CCF data from LEA memory?
It is probably in one of the gNVMemBlock, gUSSLEATempMemBlock or gUSSLEARAMReservedBlock2 but I've not yet been able to take it apart completely.
What is the variable type and alignment?
Best regards,
Kostyantyn